11/03/09 – New Toshiba Business Laptops Balance Performance, Mobility and Value
IRVINE, Calif.—Nov. 3, 2009—Toshiba's Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the availability of its new line of Satellite Pro®, Tecra® and Portégé® business laptops with Windows® 7 support. The Satellite Pro line features new screen size options in 15.6-inch, 17.3-inch diagonal display configurations as well as a 13.3-inch diagonal touch-screen display and includes performance enhancements that will appeal to cost-conscious professionals looking for a reliable PC at the right price.
More »
09/17/09 – Toshiba Launches Wireless Universal Docking Station
IRVINE, Calif. — September 17, 2009 — Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the availability of its universal dynadock™ wireless U USB docking station. Toshiba’s next generation of its dynadock™ U, a top selling universal docking station on the Internet, features wireless USB technology that eliminates the need for a cable between the docking station and laptop.
More »
07/28/09 – Toshiba Breaks Into the 3.5-inch External HDD Market
IRVINE, Calif. — July 28, 2009 — Toshiba's Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the availability of a new Toshiba 3.5-inch External HDD, marking Toshiba's first entry into the 3.5-inch external HDD business. The product offers digital consumers and business professionals a stylish and affordable back up device with dual connectivity, robust software features and up to 1TB of capacity from a trusted brand.
More »
07/16/09 – Toshiba Casts Boring and Normal Contestants
IRVINE, Calif. — July 16, 2009 — Toshiba's Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc. is proud to present the competing casts for the Toshiba Laptops reality Webcast. They are anything but boring and normal—but they all come from there. Boring, Ore. and Normal, Ill. are the two towns slated to host Toshiba's contest to determine which town's residents using Toshiba technology is the more exciting place.
More »
07/06/09 – Toshiba Sets You Free with New Marketing Campaign
IRVINE, Calif. —July 6, 2009— Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced their new “Set You Free” television, digital, print, and cinema ad campaign. Toshiba’s laptop marketing effort represents a new approach to reaching consumers beyond retail.
More »
06/02/09 – Toshiba Announces US Availability of the Toshiba mini NB205: A Mini Notebook to Envy
IRVINE, Calif. — June 2, 2009 — Toshiba's Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the Toshiba mini NB205, a compact, lightweight companion PC that makes it easy to stay connected, productive and informed while on the go. With a design hallmarked by a comfort-driven, full-sized keyboard and large touchpad, nine hours of battery life1 and a highly-stylized Texture Finish offered in a choice of colors, the mini NB205 marks the company's first entry into the U.S. mini notebook market.
More »
05/14/09 – Toshiba Brings New Satellite Pro® S300M-EZ2421 to Market
Toshiba’s Digital Products Division launched its newest Satellite Pro® S300M model, the S300M-EZ2421. This laptop is designed for business professionals looking for mobility at an affordable price. Building on its highly successful predecessor, the S300M-EZ2401, it features Genuine Windows® XP Professional, enhanced wireless capabilities, eSATA/USB Combo Sleep and Charge port, increased memory, a larger capacity hard drive, docking capabilities and a one-year international limited warranty. The Satellite Pro S300M-EZ2421 also includes Toshiba's EasyGuard® Technology with PC Health Monitor. These enhancements can help protect your laptop from theft, spills and jolts as well as continuously check the performance and functionality of a system's critical hardware components and alert users when the system is in need of a tune-up.
More »
04/21/09 – Toshiba Announces New Tecra R10-S4411
Toshiba has added the Tecra ® R10-S4411 to its business line of laptops. The new thin and light Tecra R10 laptop is an Intel ® Integrated Graphics version of the highly successful R10-S4401. The laptop features a 14.1 inch high resolution LED Backlit LCD screen and Toshiba’s Standard Three-Year International Limited Warranty. With an EPEAT ™ Gold rating, the Tecra R10 is also Energy Star 4.0 and RoHS compliant, saving on energy at all levels of use. As with all of Toshiba’s business laptops, the R10-S4411 also includes Toshiba's EasyGuard® Technology with PC Health Monitor. These enhancements can help protect your laptop from theft, spills and jolts as well as continuously check the performance and functionality of a system's critical hardware components and alert users when the system is in need of a tune-up.
More »
02/24/09 – Toshiba Technology Alert: New Portégé Tablet PCs
Toshiba expands its Portégé M750 line to deliver a full performance Tablet PC solution for the back-to-school buying season. The newest additions include the Portégé M750-S7211, Portégé M750-S7212 and Portégé M750-S7213 which offer users more options suited for their required use and budget needs. For the user who requires additional warranty coverage, the same configurations will also be available in a four-year limited warranty model. Featuring EasyGuard® Technology with PC Health Monitor, the Portégé M750 series can help protect your laptop from theft, spills and jolts as well as continuously check the performance and functionality of a systems’s critical hardware components and alert users when the system is in need of a tune up. Based on Intel® Core™ microarchitecture, the Intel® Core™2 Duo processor family is designed to provide powerful energy-efficient performance so you can do more at once without slowing down.
More »
02/10/09 – Toshiba Technology Alert: Tecra® A10-S3511, Tecra® M10-S3411
Toshiba has expanded its Tecra® line of laptops with two new models, the Tecra® A10-S3511 and Tecra® M10-S3411. The highly durable laptops are suited for the business professional with built-in security features and a standard three-year limited warranty. These high quality machines come with high resolution LCD screens, Windows Vista Business, 2GB memory, WiFi link, built-in Webcam, Bluetooth® port and Toshiba’s EasyGuard® Technology.
More »