awards & achivements
 1 of 2  Next Page »

09/18/09 – The best new gadgets for business, CNNmoney.com

"The other notebook worth mentioning is Toshiba's Portege R600. Now, unless a computer will cook and clean up after me, any price tag of more than $2,000 is absurd these days. Regardless, it was a neat product. At 2.4 pounds, Toshiba still managed to keep the optical drive in the unit. That's unheard of. It's under an inch thin, as well, and has a seven-hour battery life with a 12.1-inch screen. The two coolest features? It has no moving parts, and you can still see all your work even if direct sunlight is hitting the screen."

More »

09/18/09 – Transformers: USB drive and mouse in disguise. Toshiba team with Hasbro to create official gadgets, pocket-lint.com :

"When was the last time you saw a USB drive do the above? Bonkers right, but not as crazy as the optical mouse that turns into a dinosaur. Toshiba has teamed up with Hasbro to launch four official 1984 Transformers in the shape of a USB drive and optical mouse in time for the "Holidays", hoping to capitalise on the films and the general nostalgia for the cartoon. "

More »

08/09/09 – The 2009 Annual Report Card Awards, ChannelWeb.com

"Amid a crowded field that grows more competitive each year, solution providers awarded Toshiba the subcategory victory for Best Support and Partnership in the Notebooks and Mobile Computers category. Managing Editor, Technology, Jennifer Follett presents the trophy to Jerry Lumpkin, Vice President, Business Channel Sales, Digital Products Division."

More »

07/09/09 – Bake-off: Six Business Notebooks, ChannelWeb.com

"Toshiba has a reputation among business users as the maker of reliable, no-nonsense laptops and the Tecra R10 (left), continues the tradition with its sleek-looking silver case. Our test unit was the R10-S4401, which has a Core 2 Duo P9300, 2.26-GHz processor, with 3 GB of RAM and ran Vista Business. Weighing in at 4.34 pounds, the R10 is the heaviest of all the units we tested for this review but, again, that doesn't necessarily mean it is heavy or uncomfortable to carry around. The 14.1-inch WXGA LED backlit display is driven by an Nvidia Quadro NVS 150M GPU and is big and bright. In light of the fact that the keyboard did not give as much feedback as we prefer, the spacing and size of the keys made typing error-free and quickly made us forget about our objection. "

More »

07/09/09 – 2009 Channel Contenders: Notebooks, ChannelWeb.com

"Toshiba's Tecra A10 notebook delivers desktop computing power on a 15.4-inch notebook. The Tecra is designed for business installations and comes preloaded with Windows Vista Business Edition. Powerful Intel processors power the business line of Toshiba notebooks, and while they can be on the expensive side, the notebooks deliver business-class performance and reliability."

More »

04/09/09 – 2009 Partner Programs Guide, ChannelWeb.com

5-Star Systems & Peripherals Programs:Toshiba Preferred Partner Program

More »

01/29/09 – Toshiba Rolls Out Four New Satellite Pro S300-Series Laptops, engadget.com

"The two-year warranty further differentiates our Satellite Pro® S300 business products from the rest in the industry and is now selling for a first-time price point of $529," said Carl Pinto, vice president of Product Development & Marketing of Digital Products Division, Toshiba America Information Systems, Inc. - Joseph L. Flatley

More »

01/27/09 – Toshiba Extends Satellite Pro Notebooks To SMBs, ChannelWeb.com

“Toshiba is expanding its Satellite Pro S300 series of notebooks with four new models while making them more attractive to small business owners by dropping the entry price point to $529.” - Brian Kraemer

More »

01/27/09 – Toshiba Drops Price of Satellite Pro S300 Notebooks, Channel Insider.com

“…‘Instead of having a system that has all different pop-ups and bloatware, we have designed a very clean load for the Toshiba Satellite Pro S300…and it offers a feature that's very popular with small-business customers,’ says Cindy Zwerling, B2B product marketing manager at Toshiba America.” - Jessica Davis

More »

01/23/09 – Toshiba Tecra R10, Computer Shopper.com

“The all-new Toshiba Tecra R10-S4401 is a thin-and-light business laptop that delivers good performance and a wealth of features…We love the combo external SATA (eSATA)/USB port, which also lets you charge devices via the port even when the R10 is asleep.” - Jamie Bsales

More »

 1 of 2  Next Page »